Is there a way within Solid Edge ST10 to batch print a folder of Solid Edge Draft files?
Solution
Yes, you can use the custom batch file which gives you the ability to control batch processes within Solid Edge. You have the option to choose three types of batch processing
- Printing a directory of Draft files.
- Converting a set of files into Solid Edge. For example converting a set of DXF files into Solid Edge Draft.
- Converting Solid Edge files into another format.
This batch file can be found in the Solid Edge Custom folder:
"\Program Files\Solid Edge ST10\Custom\Batch\Bin".
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: SOLID_EDGE
Application: AUTOMATION
Version: V110.0
Function: DRAFT
Ref: 002-8002029