Details
After upgrading to ST10, ST10 will not run and the license server is showing the following errors:
FlexNet Licensing Error:-140,148
Solution
This error indicates that the Flex license server has not been updated and is an older version of Flex that is not compatible with ST10.
Upgrading the Flex software to use the Flex version delivered with the ST10 install media should resolve this error and allow ST10 to run.
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: SETUP
Version: V110.0
Function: LICENSING
Ref: 002-8002026