Details
By default JT files (.jt) are not associated to the Solid Edge application in Windows Explorer. Using 'Set your default programs' in Windows to associate JT files with Edge.exe will result in launching multiple instances of Solid Edge instead of opening the JT files into a single, already running instance of Solid Edge.
Solution
To force Windows Explorer to open JT files from Windows Explorer into a single instance of Solid Edge, add the following registry keys:
[-HKEY_CURRENT_USER\Software\Classes\.jt]
[-HKEY_CURRENT_USER\Software\Microsoft\Windows\CurrentVersion\Explorer\FileExts\.jt]
[HKEY_CURRENT_USER\Software\Classes\.jt]
@="SolidEdge.PartDocument"
[HKEY_CURRENT_USER\Software\Microsoft\Windows\CurrentVersion\Explorer\FileExts\.jt]
[HKEY_CURRENT_USER\Software\Microsoft\Windows\CurrentVersion\Explorer\FileExts\.jt\OpenWithList]
"a"="Edge.exe"
"MRUList"="a"
[HKEY_CURRENT_USER\Software\Microsoft\Windows\CurrentVersion\Explorer\FileExts\.jt\OpenWithProgids]
"SolidEdge.PartDocument"=hex(0):
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: APPLICATION
Version: V110.0
Function: OTHER
Ref: 002-8002017