Enable write access to or modifying Released status file without changing status

2021-10-06T23:52:17Z

Summary


Details

Is it possible to enable write access to or modify a Released status file without changing the status of the file or creating a new revision?

Solution

Normal Solid Edge behaviour prevents you from making changes to a file with a Released status without first changing the status of the file or creating a new revision of a file.  Using the following workaround it is possible to modify a Released status file without changing the status of the file or creating a new revision.

In the registry create the following DWORD (32-bit) value:

HKEY_CURRENT_USER\Software\Unigraphics Solutions\Solid Edge\Version 110\DEBUG\DOCMGMT_OVERRIDESTATUSCHECKFORFILEACCESS 

Set this value to = 1.

Now, whenever you open a Released status file in Solid Edge, in the Read-Only Assistant window select "Request write access" and the file will immediately become modifiable without having to change the file status or creating a new revision.  

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Version: V110.0
Function: FILE

Ref: 002-8002010

KB Article ID# PL8002010

Contents

SummaryDetails

Associated Components