You borrowed a license and you now want to return it to the server. You were unable to return the license from the client machine. Possible reasons can include:
- Errors when trying to return a borrowed license early
- Deletion or corruption of the user's profile who borrowed the license
- Hard drive failure which renders the operating system inaccessible
Solution
Only the borrowing client can return a borrowed license. There is no way to force the return of a borrowed license from the FlexLM license manager. Once the borrow period expires the license will be automatically returned to the license server pool.
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: SETUP
Version: V110.0
Function: LICENSING
Ref: 002-8002007