Details
Comparing the performance results for the same hardware using the Solid Edge Performance Test v1.0 tool and the Solid Edge Performance Test v1.2 too, the v1.2 tool shows far worse performance results than the v1.0 test results. Why?
Solution
Solid Edge Performance Test V1.2 is *not* the same as V1.0 and should not be used to compare versions of Solid Edge based on different versions of the performance tool. By that we mean the results will not be comparable because additional code was added to stress faster graphics cards in V1.2. So you should not expect the numbers from V1.0 to match V1.2. You should only compare V1.2 results against V1.2 results.
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: APPLICATION
Version: V110.0
Function: OTHER
Ref: 002-8002001