Disable auto revision or auto change triangles on drawings

2021-10-06T23:52:13Z

Summary


Details

After making changes to a model, the Solid Edge draft once updated then has automatic revision or change triangles displayed for every dimension that was modified in the model.  How to disable this?

Solution

The automatic Dimension Tracker can be disabled in the draft by selecting Tools tab -> Track Dimension Changes -> Options tab.

In the Options tab uncheck "Track changed dimensions".

For more on the Dimension tracker options see the following Solid Edge documentation:

https://docs.plm.automation.siemens.com/tdoc/se/110/se_help#uid:xid1129777:xid1325276:xid1325279:index_dimensions:xid280168:trdmch1d:trdmch2d



Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: DRAFT
Version: V110.0
Function: DIMENSIONS

Ref: 002-8001994

KB Article ID# PL8001994

Contents

SummaryDetails

Associated Components