Solid Edge Using propseed file with SEEC mapped properties

2021-10-06T23:52:12Z
DOC_MANAGEMENT

Summary


Details

Is it possible to use the propseed file with mapped properties in SEEC?

Solution

The propseed file will work with SEEC if the Solid Edge properties are not mapped to Teamcenter.

As soon as the Solid Edge properties are mapped to Teamcenter, the propseed file will no longer work with those mapped properties.

For mapped properties in SEEC, to generate a list of values for a property you must explicitly define an LOV object in Teamcenter for the mapped property.



Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V110.0
Function: SEEC

Ref: 002-8001993

KB Article ID# PL8001993

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEEC