Solid Edge Maintenance pack in "Update" folder is not automatically installed with silent install of base Solid Edge

2021-10-06T23:52:12Z
PART/SHEETMETAL

Summary


Details

With a Solid Edge maintenance pack copied into the base Solid Edge media "Solid Edge" -> "Update", running a silent install of base Solid Edge is then not automatically installing the maintenance pack as expected.  Why?



Solution

Copying a maintenance pack into the "Update" folder on the Solid Edge base media will automatically install the maintenance pack as soon as the base Solid Edge install has been completed.  However, this method only works with the GUI based Solid Edge install methods.  For a silent install, this automatic maintenance pack install method will not work.

Instead, for silent install methods, the maintenance pack silent install command should be called separately as part of the overall silent install routine.




Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: SETUP
Version: V110.0
Function: INSTALL

Ref: 002-8001991

KB Article ID# PL8001991

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FEATURES