Solid Edge Can the Solid Edge Status Bar to repositioned or relocated?

2021-10-06T23:52:11Z
PART/SHEETMETAL

Summary


Details

Can the Solid Edge Status Bar to repositioned or relocated from the bottom of the Solid Edge window to another location within the Solid Edge window?

Solution

Unfortunately the Status Bar is not a dockable element.  As such, it cannot be moved.  There are ERs requesting this functionality.

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: APPLICATION
Version: V110.0
Function: UI

Ref: 002-8001989

KB Article ID# PL8001989

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FEATURES