Is it possible to automate the KeyShot application provided with Solid Edge using Solid Edge APIs?
Solution
As KeyShot is a third-party application, you cannot automate it the same way that you would with Solid Edge.
Actually, only KeyShot 6, which is delivered with ST10 supports automation. This KeyShot automation process only supports scripting through Python 3.4.
If trying to automate Solid Edge and KeyShot, you would probably create your documents in Solid Edge using Solid Edge APIs and then call KeyShot from a command line with the Python script to automate the rendering.
For more on KeyShot scripting please see the following reference:
https://keyshot.com/scripting/doc/6.0/quickstart.htmlHardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: APPLICATION
Version: V110.0
Function: KEYSHOT
Ref: 002-8001988