Details
Dimension names are displayed instead of values.
Solution
This is because 'Show All Names' is checked for dimension. Instead this should have check 'Show All Values'. To set this select the dimension and from right mouse button menu use option 'Show All Values'. This should display dimension values.
On Right Mouse Button three related options are available:
• Show All Values : Displays the dimensional values for all the dimensions.
• Show All Formulas: Displays all dimensions in a Name=Formula format. If no formula has been defined for a dimension, it is displayed in a Name=Value format.
• Show All Names: Displays the names for all the dimensions.
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764
Product: SOLID_EDGE
Application: ASSEMBLY
Version: V110.0
Function: DIMENSIONS
Ref: 001-9105019