Aborting when translating a Solid Edge ST10 file to PDF format.

2021-10-06T23:52:06Z

Summary


Details

When translating a Solid Edge ST10 file to PDF format, getting aborted out of Solid Edge.





Solution

To resolve this, you must remove both the Printer and Driver; removing only one of these will not resolve the problem.


  • Uninstall Solid Edge 
  • Uninstall the Printer and Driver, click Control Panel 
  • Select Printers & Drivers 
    • Delete the appropriate Printer, then proceed to remove the printer driver. 
    • Right mouse click in free space under the Printers list and select Server Properties 
    • Click Drivers tab 
    • Remove the appropriate driver 
  • Re-install Solid Edge and the problem should be resolved.




Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 10_1709
Product: SOLID_EDGE
Application: TRANSLATORS
Version: V110MP6
Function: PDF

Ref: 002-8001918

KB Article ID# PL8001918

Contents

SummaryDetails

Associated Components