How to place Intermediate Components in a Formboard Drawing?

2021-10-06T23:26:19Z

Summary


Details

Using From Component, To Component and Intermediate Component, a connection can be created.


However while creating a Formboard drawing, the intermediate component goes missing.


How to place Intermediate Components in a Formboard Drawing?



Solution

There has to be an RCP (Routing Control Point) on the spline path at the point where an intermediate component is connected.


Using "Subdivide path" command it can be added if it is not exist already.



Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764
Product: NX
Application: ROUTING_ELEC
Version: V11.0.2
Function: FORMBOARD_V2

Ref: 002-8001904

KB Article ID# PL8001904

Contents

SummaryDetails

Associated Components