NX Hole Treatment Centermak is not displayed in the Flat Pattern

2021-10-06T23:26:19Z
NX for Design

Summary


Details

CenterMark is not displayed instead of holes in the Flat pattern even if the CenterMark option is selected in Flat Pattern dialog for Hole Treatment.

Solution

The CenterMark will be displayed when the diameter of the hole is lesser or equal to the entered Hole Treatment value.


Hence in the cases where the diameter of the holes are higher than the entered hole treatment value, the holes will remain as it is.



Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764
Product: NX
Application: NX_SHEET_METAL
Version: V12.0.1
Function: FLAT_PAT_FEAT

Ref: 002-8001902

KB Article ID# PL8001902

Contents

SummaryDetails

Associated Components

Sheet Metal