Solid Edge Unable to update older Holes table database in Solid Edge . . .

2021-10-06T23:52:00Z
PART/SHEETMETAL

Summary


Details

How do you update an older Holes table database from Solid Edge ST6 to Solid Edge ST10?

Solution


When updating legacy hole databases (for example a Holes.txt or Threads.txt) database, we provide a holes database converter. These two legacy databases are written to a new hole database file and are located in the ../Program Files/Solid Edge ST10/Preferences/Holes folder. Solid Edge only recognizes the hole databases that are contained in this folder. You can find the Converter utility at the following location: 

. . . /Program Files/Solid Edge ST10/Custom/HoleDatabaseConverter/bin/Hole Database Converter.exe.

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Version: V110MP6
Function: FEATURES

Ref: 002-8001833

KB Article ID# PL8001833

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FLAT_PATTERN