How to change the way hole numbers are displayed in the hole table.

2021-10-06T23:51:59Z

Summary


Details

How do you change the way hole numbers are displayed in the hole table?

Solution

: Select the Hole table
: Right Mouse Button Click > Select Properties
: Use the Options tab to specify whether you want to see hole origin or hole number in the first column of the hole table. 
: Uncheck the option 'Show origin or group name in list'
- When this option is unchecked, the group designator and delimiter are removed from the Hole column and from the hole callout annotation.

Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764
Product: SOLID_EDGE
Application: DRAFT
Version: V109MP2
Function: TABLES

Ref: 002-8001827

KB Article ID# PL8001827

Contents

SummaryDetails

Associated Components