Simcenter 3D Solutions Plotting stress vs strain from independant stress/strain results

2021-10-06T23:26:18Z
Simcenter 3D

Summary


Details

Consider the following example scenario.

NX Nastran non-linear statics (SOL 106) has been used to analyse a structure for which non-linear material properties have been defined and where the load is sufficient for the material to undergo plastic deformation.

Both stress and strain results can be plotted as a function of the load factor.  However, how to generate a stress vs strain graph of these same results?

Solution

Within the 'post-processing navigator':

Plot stress results (contour plot)

Plot stress vs load factor as an xy graph

Save the graph to an '.afu' file (say 'stress_strain.afu')

Plot strain results (contour plot)

Plot strain vs load factor as an xy graph

Save the graph to the same '.afu' file ('stress_strain.afu')

Within the 'xy function navigator':

Expand out the 'afu files - xy tabular function/associated afu/(stress_strain.afu)' item to reveal the graphs

Select both graphs, then 'rhmb, two functions' and select the second of the two options presented (function 2 -> function 1)

A stress vs strain plot will be generated

***

Alternatively, another method to create the same xy graph plot is detailed within the NX 11 Help Documentation article entitled:

Create a two function plot

Notes

KB Article ID# PL8001826

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow