March 5, 2018 Dear Solid Edge Customer: Solid Edge ST9 Microsoft Installer (MSI) Maintenance Pack 14 is available for download.
Sincerely,
The Solid Edge Team ============
Release Notes:============
Microsoft Installer (MSI) Maintenance Packs – Solid Edge ST9 Maintenance Packs are installed using Microsoft Installer (MSI) technology. Solid Edge MSI based Maintenance Packs are tracked as Installed Updates.
=============
Update Version:=============
109.00.14.03 ================
Download Location:================
ST9 Maintenance Packs can be downloaded from:
https://download.industrysoftware.automation.siemens.com/solid_edge/ST9/Maintenance_Packs/ ==========
Installation:==========
Downloadable .zip files are complete product setups. Therefore, existing versions must be uninstalled
using Uninstall a program from the Control Panel before installing the new version.
=========================================
This Maintenance Pack addresses the following PRs:=========================================
===Assembly=== PR 7877204: Open as Last Saved not working for placing assembly from part library
===Draft=== PR 9024961: Crash when copying from background sheet
PR 9041036: Unnecessary hatch is displayed when drawing data of ST4 is opened in ST9
PR 9045466: Vertical dimension changes when trying to reattach witness line endpoints
PR 8939156: The position of parentheses in the Reference Dimension is wrong
PR 9068621: Opening the ST4 drawing in ST9 change the dimension position of the ISO view
===Design Manager===PR 9024445: Prevent duplicate Filename causes a check-in error
===General===PR 9067490: Switching Windows takes many, many seconds
===Built-in Data Management===PR 9087449: Cannot change non ST9 part/file Status using SolidEdgeFileProperties API
SFB-SOLID_EDGE-8001687
Product Information: