Dear Siemens PLM Software Customer,
We are pleased to inform you that Tecnomatix controllers for "REIS, ABB, CLOOS, COMAU, DEFAULT, DENSO, DUERR, EPSON, FANUC, IGM, KAWASAKI, KUKA, NACHI, NC, PANASONIC, STAUBLI, TOOLS/OLP_TOOL, TRALLFA, UNIVERSAL, USER_INVERSES/7R_AXIS_INVERSE, USER_INVERSES/DUERR_ECOTALK_INVERSE, USER_LB_FUNCS/OLP_FUNC, YASKAWA" are available for download from https://download.industrysoftware.automation.siemens.com.
See Tecnomatix_Controller_Name_changes_log.htm for details concerning this update.
Note: This file is located in the 'Change_Logs' folder directly under the 'Robot_Controllers' folder.
Use the following steps to download.
Note: A valid WebKey account is required.
(URL: https://plmapps.industrysoftware.automation.siemens.com/webkey/)
In your browser address window enter the URL: https://download.industrysoftware.automation.siemens.com/
WebKey Username: [your WebKey user ID]
WebKey Password: [your WebKey password]
Select the Download tab
In the Product Filter area scroll down to Tecnomatix Products
Select Tecnomatix Products
Expand Product updates
Expand Planning_Applications/
Expand Robot_Controllers/
Expand V13.0/, V13.0.2/, V13.1/, V13.1.1/, V13.1.2/, V14.0/, V14.0.1/ or V14.0.2/
Expand REIS, ABB, CLOOS, COMAU, DEFAULT, DENSO, DUERR, EPSON, FANUC, IGM, KAWASAKI, KUKA, NACHI, NC, PANASONIC, STAUBLI, TOOLS/OLP_TOOL, TRALLFA, UNIVERSAL, USER_INVERSES/7R_AXIS_INVERSE, USER_INVERSES/DUERR_ECOTALK_INVERSE, USER_LB_FUNCS/OLP_FUNC or YASKAWA
Download the file(s):
Tecnomatix_13.0_REIS_ROBSTAR_64BIT_v2.4_26_02_2018.exe
Tecnomatix_13.0.2_REIS_ROBSTAR_64BIT_v2.4_26_02_2018.exe
Tecnomatix_13.1_REIS_ROBSTAR_64BIT_v2.4_26_02_2018.exe
Tecnomatix_13.1.1_REIS_ROBSTAR_64BIT_v2.4_26_02_2018.exe
Tecnomatix_13.1.2_REIS_ROBSTAR_64BIT_v2.4_26_02_2018.exe
Tecnomatix_14.0_REIS_ROBSTAR_64BIT_v2.4_26_02_2018.exe
Tecnomatix_14.0.1_REIS_ROBSTAR_64BIT_v2.4_26_02_2018.exe
Tecnomatix_14.0.2_7R_AXIS_INVERSE_64BIT_v1.1.6_23_11_2017.exe
Tecnomatix_14.0.2_ABB_RAPID_64BIT_v3.2.4_16_02_2018.exe
Tecnomatix_14.0.2_ABB_RAPID_VOLVO_64BIT_v3.12_30_01_2018.exe
Tecnomatix_14.0.2_CLOOS_CAROLA_64BIT_v1.16_17_11_2017.exe
Tecnomatix_14.0.2_COMAU_PDL_64BIT_v4.1.16_09_02_2018.exe
Tecnomatix_14.0.2_COMAU_PDL_VOLVO_64BIT_v2.6_24_11_2017.exe
Tecnomatix_14.0.2_DEFAULT_64BIT_v2.26_08_02_2018.exe
Tecnomatix_14.0.2_DENSO_PACSCRIPT_64BIT_v1.4_17_11_2017.exe
Tecnomatix_14.0.2_DUERR_ECOTALK_64BIT_v2.19_12_01_2018.exe
Tecnomatix_14.0.2_DUERR_ECOTALK_INVERSE_64BIT_v2.2_17_01_2018.exe
Tecnomatix_14.0.2_EPSON_SPEL_64BIT_v1.14_17_11_2017.exe
Tecnomatix_14.0.2_FANUC_F100_64BIT_v2.1_15_12_2017.exe
Tecnomatix_14.0.2_FANUC_RJ_64BIT_v2.34_16_02_2018.exe
Tecnomatix_14.0.2_FANUC_RJ_JAPAN_64BIT_v2.32_16_02_2018.exe
Tecnomatix_14.0.2_IGM_INS_64BIT_v1.20_23_11_2017.exe
Tecnomatix_14.0.2_KAWASAKI_AS_64BIT_v2.44_15_02_2018.exe
Tecnomatix_14.0.2_KUKA_KRC_64BIT_v3.51_08_02_2018.exe
Tecnomatix_14.0.2_KUKA_KRC_BMW_64BIT_v2.48_08_02_2018.exe
Tecnomatix_14.0.2_KUKA_KRC_VOLVO_64BIT_v2.21.4_22_12_2017.exe
Tecnomatix_14.0.2_NACHI_SLIM_64BIT_v3.4.1_22_12_2017.exe
Tecnomatix_14.0.2_NC_CODE_64BIT_v1.24_16_01_2018.exe
Tecnomatix_14.0.2_NC_CODE_BMW_64BIT_v1.15_17_11_2017.exe
Tecnomatix_14.0.2_NC_CODE_EMBRAER_64BIT_v1.5.6_17_11_2017.exe
Tecnomatix_14.0.2_NC_CODE_RIVETING_64BIT_v1.3.4_17_11_2017.exe
Tecnomatix_14.0.2_OLP_FUNC_64BIT_v1.0_12_01_2018.exe
Tecnomatix_14.0.2_OLP_TOOL_64BIT_v14.7_15_01_2018.exe
Tecnomatix_14.0.2_PANASONIC_CSR_64BIT_v1.8_17_11_2017.exe
Tecnomatix_14.0.2_REIS_ROBSTAR_64BIT_v2.4_26_02_2018.exe
Tecnomatix_14.0.2_STAUBLI_VAL_64BIT_v1.16_17_11_2017.exe
Tecnomatix_14.0.2_TRALLFA_ROBTALK_64BIT_v1.26_22_12_2017.exe
Tecnomatix_14.0.2_UNIVERSAL_URSCRIPT_64BIT_v2.8.1_16_01_2018.exe
Tecnomatix_14.0.2_YASKAWA_INFORM_64BIT_v3.60.1_13_02_2018.exe
To Install:
Place Tecnomatix_<TecnomatixVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe into a folder ($Tecnomatix/downloads is suggested), where $Tecnomatix is the full path to the Tecnomatix installation.
Run Tecnomatix_<TecnomatixVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe.
The default installation point is C:\Program Files\Tecnomatix.
If you have any issues with the installation or support of these fixes,
please contact your local GTAC support group.
Sincerely,
Siemens PLM Software
SFB-TECNOMATIX-8001665
PR N/A
Product Information: