Tiff output is different on NX8 and NX11.

2021-10-06T23:26:15Z

Summary


Details

When output tiff on NX 8 and NX 11 using the same data there are many differences.

Solution

This is a case were related to clipping. It happens when the data fell on a dot which was technically outside of the viewport so wasn't included in the rendered output. Slightly by increasing the viewport to overcome any potential clipping.
This logic is not implemented at higher resolutions as should be evident if you exported at 300dpi for example.

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: XP64_SP2
Product: NX
Application: GATEWAY
Version: V11.0.2
Function: PLOTTING

Ref: 002-8001646

KB Article ID# PL8001646

Contents

SummaryDetails

Associated Components