NX When check-mate is executed, an exception error is displayed.

2021-10-06T23:26:15Z
NX System Administration NX for Design

Summary


Details

When check-mate is executed, an exception error is displayed.Depending on the data, even if the check passes, an error occurs.
 



Solution

When certain attributes are missing the GQS gives exception errors. 
When the DCS File Log is run on the part file, the required DCS part attributes will be added, such as context and DB_PART_TYPE. When these part attributes exist, the checkmate test will not fail.

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: XP64_SP2
Product: NX
Application: TOOL_KITS
Version: V11.0.1
Function: PDL

Ref: 002-8001645

KB Article ID# PL8001645

Contents

SummaryDetails

Associated Components

Installation