February 12, 2018 Dear Solid Edge Customer: Solid Edge ST10 Maintenance Pack 4 is now available for download.
Sincerely,
The Solid Edge Team ============
Release Notes:============
Solid Edge ST10 Maintenance Packs are delivered using Microsoft Installer (MSI) technology.
Microsoft Windows 10 releases Feature Updates every six months. Microsoft does not use Windows 10 Feature Updates as an avenue to deliver security-related patches. All quality-related patches, including security and reliability hot-fixes, will continue to be delivered outside of this Feature Update process. Therefore, if your production use of Solid Edge was negatively impacted as a result of the last Microsoft Windows 10 Feature Update, you should consider configuring your Windows 10 machines to delay the deployment of Windows 10 Feature Updates. Configuring your Windows 10 machines by moving the machines into the "Semi-Annual Channel" servicing channel will delay the installation of Feature Updates for approximately four months following the initial release. During this time, you and your IT organization will have the opportunity to review the suitably of the Feature Update, including determining any negative impact, upon the applications that you use in your production environment, such as Solid Edge. This four-month window of time between Microsoft initially releasing the Feature Update to targeted machines and releasing the Feature Update for general deployment to the enterprise will also provide our development team time to review and react to changes introduced by Windows 10 Feature Updates, thereby helping keep you as productive as possible.
=====================
Maintenance Pack Version:=====================
Solid Edge ST10 MP4
Version
: 110.00.04.03 ================
Download Location:================
Solid Edge ST10 Maintenance Packs can be downloaded from:
https://download.industrysoftware.automation.siemens.com/solid_edge/ST10/Maintenance_Packs/ ==========
Installation:==========
Maintenance Pack .zip files are complete product setups. Therefore, existing versions must be uninstalled using Uninstall a program from the Control Panel.
• MSI Product Updates can be applied on top of the base release and or existing Product Update with a lesser version.
• MSI Product Updates are all inclusive, i.e. fixes delivered in MP3 include all fixes delivered in MP1 and MP2.
• MSI Product Updates calculate free disk space before installing. Please note that there have been cases where the Disk Space Computation takes several minutes to complete. Please be patient.
• MSI Product Updates can be uninstalled without having to remove the base Solid Edge product.
• Uninstalling an MSI Product Update will restore the installation to the state before the Product Update was applied.
• PLEASE NOTE: When uninstalling an MSI Product Update, the original source media, and the previous Product Update package, if any, must be available to allow the recovery of previous file versions.
• The current MSI Product Update will be the only Update listed and available for uninstallation. After the current Update is uninstalled, the previous Update will become the current Update, if there were multiple Updates installed.
• MSI Product Updates are uninstalled via the Control Panel (Uninstall a program –> View installed updates -> Uninstall).
=========================================
This Maintenance Pack addresses the following PRs:=========================================
===General===
PR 9018172: Menu / Icon load slow after installation of Windows 10 Fall Creator Update
PR 9058022: No longer able to use stylus after updating to Windows 10 Fall Creator Update
PR 8536218: Saving Solid Edge files fails when there is no disk space, should provide warning
PR 9067490: Switching between windows takes many, many seconds
PR 9079004: Solid Edge properties are missing in Windows Explorer after installing ST10MP
===Assembly===
PR 8969056: Profile relationships lose connection and do not update
PR 7601296: Physical properties, update on file save does not work
PR 8358219: Solid Edge aborts when showing sketches in assembly
PR 8993495: Reference plane does not update when linked excel variable changes
PR 9011878: frames created are totally wrong
PR 8996483: Holes are changing if OTHER holes are changed
PR 9059608: 3D Sketch displays for inactive simplified subassembly
PR 9062219: Transparency in Texture background color function does not work correctly
===Draft===
PR 8352907: Detection of paper orientation when printing does not work in ST10
PR 7927673: More than 30s to modify line width or color in a group
PR 8351407: Undesired spaces in the stacked text
PR 8356263: Cannot drag columns of block table with ALT key in 2D Model view
PR 9013569: Hole Table annotation moves to default position if one hole will be removed
PR 8957087: Coordinate dim on rotated view is incorrect
PR 9009961: A modification that succeeds in MP9 fails in MP10.
PR 9016318: Broken out section does not cut correctly
PR 9024961: Crash when copying from background sheet
PR 9041036: Unnecessary hatch is displayed when drawing data of ST4 is opened in ST9
PR 9045466: Vertical dimension changes when trying to reattach witness line endpoints
PR 9069626: Wrong units are shown in print range on Paper Print settings dialog
===Part===
PR 9008477: After creating a block the active layer does not change and hiding layers does not work
PR 9008495: Suppressed or rolled back features affects the features created previously
PR 9011611: PMI Dimension not showing Status correctly
PR 9019993: Members of FOP are opening only in preview
PR 9021121: "IF" formula doesn't work properly in Variable Table
PR 9043412: XpresRoute gives an error when using saved setting end treatment of 90 deg
PR 8935862: Failed to optimize selected geometry
PR 8981720: Recompute fails
PR 9036131: Flat pattern not creating with normal cut on lofted flange
===Translators===
PR 8356404: Some graphic components are not imported from AutoCAD
PR 8982501: Catia translator fails to open part
PR 8987714: SW drawings imported into Solid Edge are different
PR 9004389: Abort, when trying to open DXF Files
===API===
PR 9021063: Please add new method BindKeyToTopology to Occurrence/SubOccurrence object
PR 9007849: Rotate and other view manipulations become slow after execution of user API
PR 9069254: Request the SolidEdgeDocument.Name API include write/set capability
PR 9007760: Call to API methods in custom AppDomain
PR 9008679: GetLengthAtParam() throws unspecified error in ST9
===Illustrations & 3D Publisher ===
PR 9056205: Tech Pub license features do not enable D&D functionality
PR 9031948: Solid Edge Technical Publications cannot output Chinese in PDF
PR 9037247: Technical Publication update doesn't check for existing installation
===Built-in Data Management===
PR 9005799: Revision number is not automatically set in new document window using built-in
PR 9027586: Unable to revise if a dot "." is in the path name
PR 9030796: ST10 Property Manager - status greyed out
PR 9061202: Get Latest Released gets the wrong revision
===Design Manager===
PR 9058390: FOP child part incorrectly moved from Standard Parts to released
===Insight===
PR 8956565: Insight: Insert assembly copy does not allow me to create new mirrored parts
PR 9028381: Insight: SE - Last saved location is not remembered in File save dialog
===Teamcenter Integration for Solid Edge===
PR 9030895: XpresRoute failures; no Material and error displayed
PR 8950787: Open dialog Files of Type field changing.
PR 8989772: No SE save_prompt closing asm after changing occurrence property via API
PR 9019859: Custom mapped required attribute is not using the custom property from SE file
PR 8356741: TALLOG message "The New component to be added during BOM Sync is ...
PR 8541999: Failed while saving if SEEC cache folder name has Korean character
PR 8942515: Create Part in Place does not honor the material selection defined by user
PR 8970920: PDF is checked out in TC and save of draft gives non-related error
PR 9013888: SE Status User Display property not changed when status updated via automation
PR 8358182: CPD does not render custom props in case of predefined Item Type
PR 9053765: Add to Teamcenter - Interactive, Item Name / Title mapping problem (Spanish)
PR 9060879: Open draft cmd will not find .dft if there is no GRM
PR 9062383: Mass is changing from lbm to kg when saving into TC
PR 9027216: Revise is changing the author in draft files to whoever revised
PR 9065345: Where used will not find dft with no GRM in the same item rev w\linked par
SFB-SOLID_EDGE-8001597
Product Information: