Details
No. of check points are doubled when executing "Adjacent Edges" command in the latest versions.
When executing "Adjacent Edges" command, if number of check points are set as 5, the analysis result is displayed with 10 check points in the information window.
This behaviour does not occur in NX8
Solution
In 'Adjacent Edges' dialog, we are specifying number of points for each adjacent edge.
In the information window, we getting the total number of checked points for this operation.
Thus the behaviour is older versions are incorrect.
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764
Product: NX
Application: STUDIO_DESIGN
Version: V11.0.2
Function: ANALYZE
Ref: 002-8001580