NX X How to hide the display of tangent constraint icon when creating sketch curves?

2021-10-06T23:26:14Z
NX for Design

Summary


Details

When creating the sketch curves when the line and the circle touch, a tangent icon is displayed.
This icon is displayed even though "Create Inferred constraint" is turned off, it is misleading that the option might be ON.

Is there a way to hide the tangent icon when "Create Inferred constraint" is turned off?

Solution

Use Alt key while bringing the line closer to the circle the tangent icon is not displayed.





Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764
Product: NX
Application: DESIGN
Version: V11.0.2
Function: SKETCHER

Ref: 002-8001573

KB Article ID# PL8001573

Contents

SummaryDetails

Associated Components

Modeling