Solid Edge Solid Edge Draft files opening as Read Only/Released

2021-10-06T23:51:40Z
DOC_MANAGEMENT

Summary


Details

Have some Draft files that are opening as Read Only/Released.  Other draft files are not displaying this problem.

Solution

This can happen if the user creating the draft files is using a template that is managed in Insight.  All Insight managed files are set to have a "Released" status causing all new files created with the Insight managed template to have a "Released" status.  Solid Edge template files should NOT be stored in the Insight managed vault.

Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V109MP8
Function: INSIGHT

Ref: 002-8001502

KB Article ID# PL8001502

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: INSIGHT