Details
When attempting to create a new Solid Edge file to be uploaded to Teamcenter, being returned the following error message: "Teamcenter returned 000000008004A061 which SEEC does not recognize as a known error. Review the log file for further information", and the Solid Edge template files are not being downloaded to the Solid Edge client.
Solution
This problem will occur when there were multiple folders named "Solid Edge Templates" in Teamcenter.
Hardware/Software Configuration
Platform: INTEL
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V109MP9
Function: SEEC
Ref: 002-8001500