Solid Edge Parts lists are being placed in the wrong location when using Teamcenter managed Solid Edge draft files.

2021-10-06T23:51:39Z
DOC_MANAGEMENT

Summary


Details

When placing a Parts List in a draft, the parts list is attached to the cursor for placement.  The user is expecting the parts list box to be fixed over the title block automatically.  The placement functionality is controlled by the "draftlist.txt" file located in the Reports folder in Solid Edge templates.

Solution

Since this is a Solid Edge Embedded Client installation, the Solid Edge templates are cached from the Teamcenter server in the Admin/Solid Edge Templates location.  The Reports folder is not read from this location.  It is read from the local Templates\Reports location in the Solid Edge installation location or defined in File Locations in Solid Edge Options, and one of these locations needs to contain the custom "draftlist.txt" file.

Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V110MP1
Function: SEEC

Ref: 002-8001499

KB Article ID# PL8001499

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEEC