Where Used is not working as expected using indexed files

2021-10-06T23:51:39Z

Summary


Details

After upgrading to ST10 the Where Used search locations (folders) are displaying as Red in color even though the location has been indexed.  If all is correctly configured, you should have the Where Used results dialog returned without having to select locations in which to query.

Solution

This problem will occur if you do not use the Fast Search Server configuration interface to build the index, but instead build the index using the Index Options interface in Control Panel.  

Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V110MP1
Function: BUILT_IN

Ref: 002-8001498

KB Article ID# PL8001498

Contents

SummaryDetails

Associated Components