Details
Unable to run Initialize Insight Services successfully. Returning the following error message: "The operation returned HTTP Error 401. This can happen when the IIS web site uses Integrated Authentication as described by MicroSoft Support Knowledgebase Article ID: 89861. Consider the details in this article and then retry the operation."
Solution
Make sure that Insight Server is installed on the C drive. It canot be installed on other drives.
Hardware/Software Configuration
Platform: INTEL
OS: window
OS Version: 2012_R2
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V109MP11
Function: INSIGHT
Ref: 002-8001487