Solid Edge The administrator is experiencing an error message when upgrading the Solid Edge SP Server software

2021-10-06T23:51:38Z
DOC_MANAGEMENT

Summary


Details

Upgrading the Solid Edge SP Server was returning the following error message when selecting to close the install dialog and start the Configure Solid Edge SP Server: "There is a problem with the Solid Edge SP Server installation and the Solid Edge SP web solutions were not deployed correctly.  Make sure the Sharepoint Timer service is running and then re-install Solid Edge SP Server."

Solution

When upgrading an existing installation, you need to use the same login last used to install and configure Solid Edge SP server.

Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 2012_R2
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V109MP6
Function: SESP-EC

Ref: 002-8001485

KB Article ID# PL8001485

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: OTHER