Details
If you want to draw a line in a Sketch or Draft with an angle that is a multiple of 15° (15, 30, 45, 60, 75, 90, 105, etc.), you can type in directly the desired value - is there a quicker solution?
Solution
Place the first point of the line, then press the <Shift> key and when moving the mouse you will notice that Solid Edge proposes all the multiple angles of 15°.
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: DRAFT
Version: V110MP3
Function: 2D_DRAWING_TOOL
Ref: 002-8001321