) In a test environment, nxmgr user is unable to open a part.
) Error dialog shows :
Open
Could not open 000045/A;1.
The following files could not be loaded, causing this open to fail:
000045/A;1 - An error occurred while downloading/uploading a file. Please check your FMS settings.

) NX syslog shows :
+++ download failed with message Unrecognized FMS error: -9009 TRY AGAIN 1
*** EXCEPTION: Error code 940053 in ...\ugmgr_fms.c ...
+++ FCC_DownloadFilesFromPLM failed with status: Unrecognized FMS error: -9009
.
.
Error downloading files: 940053
) However, checking the NX syslog, FMS_HOME *is* set correctly.
Solution
) In this test environment, an old fcc process (java.exe) was still running.
) To resolve, user ran the following in a command prompt window,
after verifying the FMS_HOME environment variable was set correctly.
cd /d %FMS_HOME%
bin\fccstat -restart
) Afterwards, the part opened fine in nx/manager.
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: NXMANAGER
Version: V11.0.2
Function: FILE_OPEN
Ref: 002-8001249