NX Multi-Field Key enabled with NX Manager

2021-10-06T23:26:12Z
NX for Design

Summary


Details

MultiField Key configured with 4 domains. Send an object to NX and ger error:
 
 NX Initialization Error
 
 The domain set as value of preference TC_MFK_DEFAULT_DOMAIN
 must contain item_id as its only key.
 Item domain contains the following keys"
 item_id,d4_CageCode,d4_Site



Solution

GTAC duplicated the error when the Teamcenter preference TC_MFK_DEFAULT_DOMAIN was set to an Item type with multiple attributes in the 'MultiFieldKey' Business Object Constant. The NX 11.0.2 Teamcenter Integration for NX - Multifield Key specifies that the Teamcenter default domain having a single attribute: item_id. 

To resolve the error, the TC_MFK_DEFAULT_DOMAIN preference was set to the COTS Item Type, with its 'MultiFieldKey' Business Object Constant is {item_id}. I the updated the NX PAX files to default to my MFK Item Type.



Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V11.0.2
Function: FILE_NEW

Ref: 002-8001245

KB Article ID# PL8001245

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX