How to remove 'mm' (Unit) from Hole Table in Solid Edge ST10?

2021-10-06T23:51:29Z

Summary


Details

How we can remove the unit (mm) from hole table in ST-10?
User wants hole table same as from Solid Edge ST-9.
 



Solution

User need to select 'No Units' (/NU) option in Column Property Text from Hole table properties.


The 'No Units' option would be available in Hole Table Properties > Select Column > In Property Text: Click in between property text > Format... button will be get activated > Select [Format...] > Select [ ] No units (/NU). OR add '/NU' in the property text.


Eg: For 'Size' column default property text would be %HS


Edit the property text as '%{%HS/NU}'; it will remove units 'mm' from the selected column.



Notes and References

IR#9050216

Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: SOLID_EDGE
Application: DRAFT
Version: V110.0
Function: TABLES

Ref: 002-8001216

KB Article ID# PL8001216

Contents

SummaryDetails

Associated Components