When user installs standard parts administrator, he gets the error message:-
Message displayed: "
Error 1606.Could not access network location
\\XYZ\ABC\SolidEdgeStandardParts."
On clicking Cancel, user is not asked to provide an alternate path and the installation process ends.
Solution
Create (if deleted) or share (if unshared) the remembered folder temporarily and change the path later once installation process continues.
Installation will then continue after the old path is found and then user can select a new path.
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764
Product: SOLID_EDGE
Application: EXTERNAL_APPS
Version: V110.0
Function: STANDARD_PARTS
Ref: 002-8001214