NX The [Folder] field of the [New Item] dialog box becomes blank in NX manager file>new

2021-10-06T23:26:12Z
NX for Design

Summary


Details

Steps to Duplicate:
====================
(1)Start Native-NX.
(2)Select [Menu] - [File] - [New].
(3)[Name] Enter an arbitrary value in the [Folder] field and click [OK].
(4)Select [Menu] - [File] - [Exit].
(5)Start Teamcenter.
(6)Start TC-NX.
(7)Select [Menu] - [File] - [New] - [Item].






Verified result:
================
The [Folder] field of the [New Item] dialog box is blank.
Selecting anu TC folder and closing the UI and again opening it shows blank field again

Solution

There is workaround for this issue: Reset Dialog Memory from NX [File >> Preferences >> User Interface >> Options Tab >> press "Reset Dialog Memory" button]. This is one time activity, if user is moving from older NX version to NX11 or later

Notes and References

PR#9026817

Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V11.0
Function: FILE_NEW

Ref: 002-8001196

KB Article ID# PL8001196

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX