About specification of Multi-Select Rule.

2021-10-06T23:26:12Z

Summary


Details

1. Open NX. Create a simple assembly having one component. Make the component work part. 
2. Create a simple block, line, point, etc. in the component. 
3. Set the setting as below. 
[Menu -> Preferences -> Selection -> Selection Rule - Inside] 
Select block or line or point of component by Rectangle selection. 
The component will also be selected in the Assembly Navigator. 



Solution

When in global selection (not in a command) and selection scope set to Entire Assembly, a component can be selected via a rectangle/lasso/circle select gesture by simply enclosing at least one member/object of the component. 
In other words, for each object enclosed by the gesture, if the object is a member of a component, the object is promoted to its owning component. In this scenario, the component (and not the object) is selected. 



Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V11.0.2
Function: SELECTION

Ref: 002-8001101

KB Article ID# PL8001101

Contents

SummaryDetails

Associated Components