Dear Siemens PLM Software Customer,
We are pleased to inform you that RobotExpert controllers for "DEFAULT, STAUBLI, ABB, CLOOS, DENSO, EPSON, IGM, KAWASAKI, KUKA, NC, PANASONIC, UNIVERSAL, YASKAWA, COMAU, FANUC, TOOLS/OLP_TOOL" are available for download from:
https://download.industrysoftware.automation.siemens.com.
See RobotExpert_Controller_Name_changes_log.htm for details
concerning this update.
Note: This file is located in the 'Change_Logs' folder directly
under the 'Robot_Controllers' folder.
Use the following steps to download.
Note: A valid WebKey account is required.
(URL: https://plmapps.industrysoftware.automation.siemens.com/webkey/)
In your browser address window enter the URL: https://download.industrysoftware.automation.siemens.com/
WebKey Username: [your WebKey user ID]
WebKey Password: [your WebKey password]
Select the Download tab
In the Product Filter area scroll down to Tecnomatix Products
Select Tecnomatix Products
Expand Product updates
Expand RobotExpert/
Expand Robot_Controllers/
Expand V12.1/, V13.0/, V13.0.1/, V13.0.2/, V13.1/, V13.1.1/, V13.1.2/, V14.0/ or V14.0.1/
Expand DEFAULT, STAUBLI, ABB, CLOOS, DENSO, EPSON, IGM, KAWASAKI, KUKA, NC, PANASONIC, UNIVERSAL, YASKAWA, COMAU, FANUC or TOOLS/OLP_TOOL
Download the file(s):
RobotExpert_12.1_DEFAULT_64BIT_v2.21_17_11_2017.exe
RobotExpert_12.1_STAUBLI_VAL_64BIT_v1.16_17_11_2017.exe
RobotExpert_13.0_DEFAULT_64BIT_v2.21_17_11_2017.exe
RobotExpert_13.0_STAUBLI_VAL_64BIT_v1.16_17_11_2017.exe
RobotExpert_13.0.1_DEFAULT_64BIT_v2.21_17_11_2017.exe
RobotExpert_13.0.1_STAUBLI_VAL_64BIT_v1.16_17_11_2017.exe
RobotExpert_13.0.2_DEFAULT_64BIT_v2.21_17_11_2017.exe
RobotExpert_13.0.2_STAUBLI_VAL_64BIT_v1.16_17_11_2017.exe
RobotExpert_13.1_DEFAULT_64BIT_v2.21_17_11_2017.exe
RobotExpert_13.1_STAUBLI_VAL_64BIT_v1.16_17_11_2017.exe
RobotExpert_13.1.1_DEFAULT_64BIT_v2.21_17_11_2017.exe
RobotExpert_13.1.1_STAUBLI_VAL_64BIT_v1.16_17_11_2017.exe
RobotExpert_13.1.2_DEFAULT_64BIT_v2.21_17_11_2017.exe
RobotExpert_13.1.2_STAUBLI_VAL_64BIT_v1.16_17_11_2017.exe
RobotExpert_14.0_ABB_RAPID_64BIT_v2.121.1_17_11_2017.exe
RobotExpert_14.0_CLOOS_CAROLA_64BIT_v1.16_17_11_2017.exe
RobotExpert_14.0_DEFAULT_64BIT_v2.21_17_11_2017.exe
RobotExpert_14.0_DENSO_PACSCRIPT_64BIT_v1.4_17_11_2017.exe
RobotExpert_14.0_EPSON_SPEL_64BIT_v1.14_17_11_2017.exe
RobotExpert_14.0_IGM_INS_64BIT_v1.19_17_11_2017.exe
RobotExpert_14.0_KAWASAKI_AS_64BIT_v2.38_17_11_2017.exe
RobotExpert_14.0_KUKA_KRC_64BIT_v3.46.1_17_11_2017.exe
RobotExpert_14.0_NC_CODE_64BIT_v1.19.1_17_11_2017.exe
RobotExpert_14.0_PANASONIC_CSR_64BIT_v1.8_17_11_2017.exe
RobotExpert_14.0_STAUBLI_VAL_64BIT_v1.16_17_11_2017.exe
RobotExpert_14.0_UNIVERSAL_URSCRIPT_64BIT_v2.7_17_11_2017.exe
RobotExpert_14.0_YASKAWA_INFORM_64BIT_v3.56_17_11_2017.exe
RobotExpert_14.0.1_ABB_RAPID_64BIT_v2.121.1_17_11_2017.exe
RobotExpert_14.0.1_CLOOS_CAROLA_64BIT_v1.16_17_11_2017.exe
RobotExpert_14.0.1_COMAU_PDL_64BIT_v4.1.4_17_11_2017.exe
RobotExpert_14.0.1_DEFAULT_64BIT_v2.21_17_11_2017.exe
RobotExpert_14.0.1_DENSO_PACSCRIPT_64BIT_v1.4_17_11_2017.exe
RobotExpert_14.0.1_EPSON_SPEL_64BIT_v1.14_17_11_2017.exe
RobotExpert_14.0.1_FANUC_RJ_64BIT_v2.29_10_11_2017.exe
RobotExpert_14.0.1_IGM_INS_64BIT_v1.19_17_11_2017.exe
RobotExpert_14.0.1_KAWASAKI_AS_64BIT_v2.38_17_11_2017.exe
RobotExpert_14.0.1_KUKA_KRC_64BIT_v3.46.1_17_11_2017.exe
RobotExpert_14.0.1_NC_CODE_64BIT_v1.19.1_17_11_2017.exe
RobotExpert_14.0.1_OLP_TOOL_64BIT_v14.4.1_24_10_2017.exe
RobotExpert_14.0.1_PANASONIC_CSR_64BIT_v1.8_17_11_2017.exe
RobotExpert_14.0.1_STAUBLI_VAL_64BIT_v1.16_17_11_2017.exe
RobotExpert_14.0.1_UNIVERSAL_URSCRIPT_64BIT_v2.7_17_11_2017.exe
RobotExpert_14.0.1_YASKAWA_INFORM_64BIT_v3.56_17_11_2017.exe
To Install:
Place RobotExpert_<RobotExpertVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe
into a folder ($Tecnomatix/downloads is suggested).
Run RobotExpert_<RobotExpertVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe.
Where $Tecnomatix is the full path to the RobotExpert installation.
The default installation point is C:\Program Files\Tecnomatix.
If you have any issues with the installation or support of these fixes,
please contact your local GTAC support group.
Sincerely,
Siemens PLM Software
SFB-TECNOMATIX-8001093
Product Information: