The properties dialog for hole tables created in ST10 no longer displays the Notes and Tolerances icon, so is there another way to edit the Notes and Tolerances in the table?
Solution
Yes, there is another way. Follow these steps to edit the Notes and Tolerances in ST10:
- Double click on the Holes table.
- To allow cell override, right click on a column header and select Allow Cell Overrides from the list.
- Double click a cell to edit the contents.

Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: DRAFT
Version: V110.0
Function: TABLES
Ref: 002-8001062