You may have noticed that the command menu for Hole Tables does not include the
Notes and Tolerances icon since ST10. That does not mean we lost this functionality.
Solution
Defining tolerances for holes is now part of the formatting of property text.

If you can recall the formatting shortcuts like
/NU, /ST, you can just key them in directly. If you need assistance with this you can access the formatting menu shown above from the
Columns tab and on the
Callouts tab inside the Hole Table properties. The
Format button becomes active as soon as you select a property.


The property text
%DI %{%HS/NU/ST+0,2^+0,1} %ZH in this example of the hole callout for simple holes results in the following output.

Use the
Data tab in the Hole Tablesproperties and
Allow Cell Override if you do not want the same tolerance for all simple holes.
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: DRAFT
Version: V110.0
Function: TABLES
Ref: 002-8001061