Installing ST10 Standard Parts on Windows 10

2021-10-06T23:51:20Z

Summary


Details

Installing Standard Parts for ST10 on Windows 10 can have problems which may be due to a conflict between versions (Windows/sql/Solid Edge/…) or updates/fixes.

The symptoms are that usually Configuration Manager and/or Administrator will not start, and often there is a message about an invalid/missing .sac-file.



Solution

Following steps should work:

1) In Windows Explorer, navigate to Standard Parts Installation Setup Folder, usually named "Standard Parts Administration".
2) Navigate to "..\Standard Parts Administration\ISSetupPrerequisites\Microsoft SQL Server 2012 Express for SE".
3) Start "SQLEXPR_x64_ENU.exe", install SQL Server using all defaults.
4) Navigate to "..\Standard Parts Administration\ISSetupPrerequisites\Microsoft SQL Server 2012 Express LocalDB for SE".
5) Start "SqlLocalDB.exe", using all defaults.
6) Navigate to "..\Standard Parts Administration".
7) Start "setup.exe" to install Standard Parts.  Make sure that you install with administrator rights.

Afterwards you should be able to start Solid Edge and to use the Standard Parts.

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: EXTERNAL_APPS
Version: V110.0
Function: STANDARD_PARTS

Ref: 002-8001048

KB Article ID# PL8001048

Contents

SummaryDetails

Associated Components