November 28, 2017 Dear Solid Edge Customer: Solid Edge ST10 Maintenance Pack 3 is now available for download.
Sincerely,
The Solid Edge Team ============
Release Notes:============
Solid Edge ST10 Maintenance Packs are delivered using Microsoft Installer (MSI) technology.
=====================
Maintenance Pack Version:=====================
Solid Edge ST10 MP3
Version
: 110.00.03.03 ================
Download Location:================
Solid Edge ST10 Maintenance Packs can be downloaded from:
https://download.industrysoftware.automation.siemens.com/solid_edge/ST10/Maintenance_Packs/ ==========
Installation:==========
Maintenance Pack .zip files are complete product setups. Therefore, existing versions must be
uninstalled using Uninstall a program from the Control Panel.
• MSI Product Updates can be applied on top of the base release and or existing Product Update with a lesser version.
• MSI Product Updates are all inclusive, i.e. fixes delivered in MP3 include all fixes delivered in MP1 and MP2.
• MSI Product Updates calculate free disk space before installing. Please note that there have been cases where the Disk Space Computation takes several minutes to complete. Please be patient.
• MSI Product Updates can be uninstalled without having to remove the base Solid Edge product.
• Uninstalling an MSI Product Update will restore the installation to the state before the Product Update was applied.
• PLEASE NOTE: When uninstalling an MSI Product Update, the original source media, and the previous Product Update package, if any, must be available to allow the recovery of previous file versions.
• The current MSI Product Update will be the only Update listed and available for uninstallation. After the current Update is uninstalled, the previous Update will become the current Update, if there were multiple Updates installed.
• MSI Product Updates are uninstalled via the Control Panel (Uninstall a program –> View installed updates -> Uninstall).
===============
E-mail Notification: ===============
To receive direct e-mail notifications for new Solid Edge Maintenance Packs, subscribe to the SFBmail notification.
For details on initiating your email subscription navigate to:
http://support.industrysoftware.automation.siemens.com/general/email.shtml =========================================
This Maintenance Pack addresses the following PRs:=========================================
===Part/Profile/Sheet Metal===
PR 8000869: Solid Edge freezes while sketching
PR 8999431: behavior of the shortcut key is incorrect
PR 8935713: Path length of file location is causing a crash on file save
PR 9003531: Solid Edge ST10 German with MP1 starts with the English User Interface
PR 8949583: API SEInstallData Object can't be instantiated anymore from a 32-bit application
===Assembly===
PR 7643671: Saving FOA subassembly with Dynamic Configuration only creates cfg
PR 8989535: Animation with detect collision aborts
PR 8998894: running the TestSEInterference macro aborts with an error
PR 9003531: Solid Edge ST10 German with MP1 starts with the English User Interface
===Draft===
PR 8987166: Printing a drawing with shaded views is incorrect
PR 8999672: Mass value of two adjustable components are not listed in part list
PR 8353804: The Create 3D command is disabled
PR 9009806: Wrong title displayed in Excel in this workflow
===Translators===
PR 8993927: Parasolid file crashes Solid Edge when opened
PR 8976936: Parasolid translation truncates the surface model filenames
===SE SP===
PR 8346838: BOM reports are missing files
===Teamcenter Integration for Solid Edge===
PR 8992417: Properties in Property manager are locked when a file has a Teamcenter Status assigned
===Built-in Data Management===
PR 8967032: SE properties are not localized in Windows Explorer
===Design Manager===
PR 9015512: Changing Document Number in Design Manager also changes Filename
===Illustrations & 3D Publisher ===
PR 8349174: SE 3D publishing produces wrong output file name
SFB-SOLID_EDGE-8001038
Product Information: