How Part Stock and Wall Stock Settings Affect Amount of Side Stock left in a Floor Wall Operation

2021-10-06T23:26:10Z

Summary


Details

Part Stock is set to 1mm in a Floor Wall Operation and Wall Stock is set to 0.  When will the Part Stock value be used to add the side stock, and when will the Wall Stock value be used to finish the wall?


Stock.JPG 37.58 KB

Solution

At first no Wall Geometry is selected in the Operation either using the Specify Wall Geometry icon or by checking on the Automatic Walls option.


1.JPG 81.5 KB
When the operation is generated the tool will offset by the value set in Part Stock because no Wall Geometry has been selected.


2.JPG 35.35 KB

If Wall Geometry is selected, NX will use the value set in Wall Stock instead of the Part Stock value.  Simply checking on the Automatic Walls option will cause Wall Geometry to be selected. The geometry can be selected manually using the Specify Wall Geometry option.


3.JPG 62.03 KB

Now that the Wall Geometry has been selected the Wall Stock value will be used. In this example the 0 stock value will cause the tool to cut right up to the wall.


4.JPG 30.85 KB

Notes

KB Article ID# PL8001022

Contents

SummaryDetails

Associated Components