Dear Siemens PLM Software Customer,
We are pleased to inform you that RobotExpert controllers for "ABB, DEFAULT, FANUC, KUKA, TOOLS/OLP_TOOL"
are available for download from
https://download.industrysoftware.automation.siemens.com.
See RobotExpert_Controller_Name_changes_log.htm for details
concerning this update.
Note: This file is located in the 'Change_Logs' folder directly
under the 'Robot_Controllers' folder.
Use the following steps to download.
Note: A valid WebKey account is required.
(URL: https://plmapps.industrysoftware.automation.siemens.com/webkey/)
In your browser address window enter the URL: https://download.industrysoftware.automation.siemens.com/
WebKey Username: [your WebKey user ID]
WebKey Password: [your WebKey password]
Select the Download tab
In the Product Filter area scroll down to Tecnomatix Products
Select Tecnomatix Products
Expand Product updates
Expand RobotExpert/
Expand Robot_Controllers/
Expand V11.1/
Expand ABB or DEFAULT or FANUC or KUKA or TOOLS/OLP_TOOL
Download the file(s):
RobotExpert_11.1_ABB_RAPID_32BIT_v2.118_05_10_2017.exe
RobotExpert_11.1_ABB_RAPID_64BIT_v2.118_05_10_2017.exe
RobotExpert_11.1_DEFAULT_32BIT_v2.19_05_10_2017.exe
RobotExpert_11.1_DEFAULT_64BIT_v2.19_05_10_2017.exe
RobotExpert_11.1_FANUC_RJ_32BIT_v2.26_05_10_2017.exe
RobotExpert_11.1_FANUC_RJ_64BIT_v2.26_05_10_2017.exe
RobotExpert_11.1_KUKA_KRC_32BIT_v3.44_05_10_2017.exe
RobotExpert_11.1_KUKA_KRC_64BIT_v3.44_05_10_2017.exe
RobotExpert_11.1_OLP_TOOL_32BIT_v14.3.3_05_10_2017.exe
RobotExpert_11.1_OLP_TOOL_64BIT_v14.3.3_05_10_2017.exe
To Install:
Place RobotExpert_11.1_Controller_Name_NNBIT_vVV_MM_DD_YYYY.exe
into a folder ($Tecnomatix/downloads is suggested).
Run RobotExpert_11.1_Controller_Name_NNBIT_vVV_MM_DD_YYYY.exe.
Where $Tecnomatix is the full path to the RobotExpert installation.
The default installation point is C:\Program Files\Tecnomatix.
If you have any issues with the installation or support of these fixes,
please contact your local GTAC support group.
Sincerely,
Siemens PLM Software
SFB-TECNOMATIX-8000997
Product Information: