Solid Edge Solid Edge ST9 - Maintenance Pack 12 Announcement

2021-10-07T00:09:56Z
SE_BETA SE_TSS DOC_MANAGEMENT FLOEFD 3D-SKETCH SIMULATION Teamcenter Share TECH_PUB ASSEMBLY APPLICATION PART/SHEETMETAL TRANSLATORS DRAFT SETUP

Summary


Details

November 20, 2017
 
Dear Solid Edge Customer: 
  
Solid Edge ST9 Microsoft Installer (MSI) Maintenance Pack 12 is available for download.
 
Sincerely,
The Solid Edge Team 
 
 
============
Release Notes:
============
 
Microsoft Installer (MSI) Maintenance Packs – Solid Edge ST9 Maintenance Packs are delivered as and
installed using Microsoft Installer (MSI) technology. Solid Edge MSI based Maintenance Packs are tracked 
as Installed Updates.
 
=============
Update Version:
=============
 
109.00.12.03
 
================
Download Location:
================
 
ST9 Maintenance Packs can be downloaded from:
 
   https://download.industrysoftware.automation.siemens.com/solid_edge/ST9/Maintenance_Packs/
 
==========
Installation:
==========
 
Maintenance Pack .zip files are complete product setups. Therefore, existing versions must be 
uninstalled using Uninstall a program from the Control Panel.
 
• MSI Product Updates can be applied on top of the base release and or existing Product Update 
  with a lesser version.
 
• MSI Product Updates are all inclusive, i.e. fixes delivered in MP3 include all fixes delivered
  in MP1 and MP2.
 
• MSI Product Updates calculate free disk space before installing. Please note that there have 
  been cases where the Disk Space Computation takes several minutes to complete. Please be patient.
 
• MSI Product Updates can be uninstalled without having to remove the base Solid Edge product.
 
• Uninstalling a MSI Product Update will restore the installation to the state before the Product 
  Update was applied.
 
• PLEASE NOTE: When uninstalling a MSI Product Update, the original source media and the previous 
  Product Update package, if any, must be available to allow the recovery of previous file versions.
 
• The current MSI Product Update will be the only Update listed and available for uninstallation. 
  After the current Update is uninstalled, the previous Update will become the current Update, if 
  there were multiple Updates installed.
 
• MSI Product Updates are uninstalled via the Control Panel (Uninstall a program –> View installed 
  updates -> Uninstall).
 
===============
E-mail Notification: 
===============
 
To receive direct e-mail notifications for new Solid Edge Maintenance Packs, subscribe to the SFBmail 
notification.
 
For details on initiating your email subscription navigate to: 
http://support.industrysoftware.automation.siemens.com/general/email.shtml 
 
=========================================
This Maintenance Pack addresses the following PRs:
=========================================
 
===Part/Profile/Sheet Metal===
PR-8993184 & 8991276: Solid Edge crashes when select a face to extrude in synchronous mode  
PR-8000869 Solid Edge freezes while sketching  
PR-8993927 Parasolid file crashes Solid Edge when opened V109
PR 8935713: Max path length of file location
 
===Assembly=== 
PR 9009522: Physical Property Manager shows different results vs Physical Property Dialog 
PR 8944800: Differing Physical Property dialog values based on the level the assembly was opened
                                                                                                                                                           
===Draft=== 
PR 8987166: Print problems with shaded views
 
===Translators===
PR 8997333 AutoCAD translation issue -Text location changes
 
===API===
PR 9009806 Wrong title displayed in Excel in this workflow
 
===General===
PR 8999431 The behavior of the shortcut key is incorrect
 
===SE SP===
PR 8346838: BOM Reports are missing files
 
===Teamcenter Integration for Solid Edge===
PR 8992417: Properties in Property manager are locked when file have a TC Status assigned
 

SFB-SOLID_EDGE-8000993
Product Information:
  • Product: SOLID_EDGE

KB Article ID# PL8000993

Contents

SummaryDetails

Associated Components

SE_BETA