How to disable license borrowing function for all users ?

2021-10-06T23:26:10Z

Summary


Details

Since license borrowing functionality is present by default in the license file (SFB-All-11151) , how can I disable it ?

Solution

In order to disable license borrowing for all license features you can either :
- remove the whole borrowing feature line or comment it with a # character in the license file :
  #INCREMENT borrowing ugslmd 32.0 permanent 1 VENDOR_STRING="For \

- use a license option file and add the following line in this option file:
    INCLUDE borrowing USER dummy_user
  This will prevent all other users than "dummy_user" to borrow a license.



Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSTEM
Version: V11.0
Function: SYSTEM_TOOLS

Ref: 002-8000933

KB Article ID# PL8000933

Contents

SummaryDetails

Associated Components