The FrameComponentsUtility.exe utility is not working with ST10.
Solution
The FrameComponentsUtility.exe is deprecated with ST10. This FrameComponentsUtility.exe was originally a VB6 32-bit utility. Solid Edge ST10 is now only 64-bit so this macro will no longer run with ST10.
In future releases this FrameComponentsUtility.exe will be removed.
Going forward you should use the "
Frame Origin" command instead.
For more on the "Frame Origin" command:
https://docs.plm.automation.siemens.com/tdoc/se/110/se_help/#uid:xid667562Hardware/Software Configuration
Platform: na
OS: n/a
OS Version: n/a
Product: SOLID_EDGE
Application: ASSEMBLY
Version: V110.0
Function: FRAME
Ref: 002-8000926