Move Face command fails with a certain set of faces with following warning:
![](/kbassets/PL8000894/8a0a75cc8eb4bea97fe01128e8526c531caaa898471416d2d73e4e2c3bd4.jpg)
Solution
The failure could be due to an incorrect "side face" extension option that is used. NX sets soft extension as default. It produces a result with better continuity when successful, but the success rate of the option is lower than the linear option.
In case of a Move Face failure, the user can try setting the Preferences -> Modeling -> Freeform -> Surface Extension Method from Soft to Linear. Repeat the Move Face operation after the change.
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: DESIGN
Version: V11.0
Function: SYNC_MODEL
Ref: 002-8000894