Details
Opening a pre NX11 prt file containing an Isocline Curve feature; when editing this feature, it shows a different dialog than editing an Isocline Curve feature created from NX11.
Why do these isocline curve features have a different Edit Parameters dialog?
Solution
Pre NX11 isocline curves are edited with its original dialog, but can be edited with the new NX11 dialog box after using the Renew Feature command.
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: DESIGN
Version: V11.0
Function: CURVE
Ref: 002-8000675